Dual Motion Safety Switches are available in two standard circuit options: OFF (locked)-None-ON and ON (locked)-None-ON. The locked safety feature requires two motions from the operator to place the actuator in the unlocked position. In locked position, pressure must be applied on the actuator forward and additional force in an upward motion for the switch to move to the unlocked position. Once unlocked, the switch can easily be moved back into the locked position.
Technical support
Phone: 866-309-9640
Fax: 828-651-0520
e-mail: orderentryVCBU@eaton.com