Crouse-Hinds series grounding plates (1/2" through 1") and insulated bushings (1/2" through 3") permit the use of the conduit as the grounding circuit. Both types have set screws and ground wire terminals.
Four is the maximum number of items in the comparison tool.
A minimum of two items are required to use the comparison tool.
Sorry, we can't get that information right now.