When the installation calls for something that doesn’t require the load-bearing capacity of Eaton’s standard B-Line series strut system, the answer is likely to be the B-Line series mini channel system. This mini metal strut system with fittings is an economical method for supporting light load requirements. For example, it can be used as a mini electrical strut system or mounted inside an enclosure.
The important features of each B-Line series mini channel include:
B-Line series aluminum mini strut channel systems are also available.
Unless otherwise noted on the drawings, all fittings feature these dimensions:
Used in conjunction with B-Line series strut system, B-Line series mini channels and fittings are the best choice for lighter loads.
A complete listing of channels, fittings and specifications is available in the B-Line section of the catalog.
Standard finishes: electro-plated zinc, Dura Green